Frequency Hopping Analysis (MB-OFDM)

Menu Path: Analysis > MB-OFDM Demod Properties > Advanced tab

Default: Hopped (See MB-OFDM Standard Setups/Presets Table.)

Range: Hopped, Not Hopped, and Force FFI

The Frequency Hopping Analysis function provides the capability for non-standard signals (not hopped) to be measured. An example of a non-standard signal is the baseband receiver signal. The default for Frequency Hopping Analysis is Hopped for standard measurements.

Measurements with standard signals:

Measurements with non-standard signals:

See Also

MB-OFDM Modulation Overview

Lengths, Intervals, and Offsets (MB-OFDM)

Using Standard Setups/Presets (MB-OFDM)

Advanced Tab (MB-OFDM Demod Properties)