Band Packet Summary (MB-OFDM)
Composite table provides measurement and analysis information unique to the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. Band Packet Summary trace. See Available Band Packet Summary Table Data for detailed information.
See Also
Available Band Packet Summary Data (MB-OFDM)