Inst Ch Frequency Response (MB-OFDM)
The Comp is the non-averaged Composite Ch Frequency Response trace data. If averaging is on, the Inst Ch Frequency Response does not show the effects of averaging.
The composite result is computed only when performing FFI analysis (TFCs 5 - 7) or TFI/TFI2 analysis when Frequency Hopping Analysis is set to Force FFI. For hopped signals, there will be no results and the error message DATA? will display.
See Also
Ch Frequency Response (Composite) (MB-OFDM)
Available Trace Data (MB-OFDM)