Tone Nulling Status (MB-OFDM)
shows which carriers have been "nulled" (removed) per the standard. See About Opt BHB: Multiband-OFDM. A subcarrier has a value of 1 if it is used and a value of 0 if it is nulled as determined by whether the power is above or below the tone nulling threshold. The tone nulling threshold can be entered in the text box. Up to 26 of the 122 subcarriers in each band may be selectively disabled (not transmitted). The following is an example of a tone nulled display.
The checkbox in the of dialog box must be selected for data to be available.
See Also
Available Trace Data (MB-OFDM)