Enable Tone Nulling (MB-OFDM)
Clear (See MB-OFDM Standard Setups/Presets Table.)
Select the checkbox to turn on the tone nulling detection.
The sets the relative magnitude level which decides whether to consider a subcarrier "nulled" or not. The range is 0 dB to -100 dB with a default of -10 dB. The results of the tone nulling are displayed in the Tone Nulling Status trace. If is cleared, there will be no data in the trace.
See Also
Advanced Tab (MB-OFDM Demod Properties)
Format Tab (MB-OFDM Demod Properties)
Time Tab (MB-OFDM Demod Properties)
Packet Tab (MB-OFDM Demod Properties)