Data From (Measurements tab)

The Data From button is used to specify the data source (real Hardware or a Recording). There are Data From buttons that apply to all measurements (in the Multi-Measurement Control toolbar) and a Data From button for each individual measurement (in the measurement row).

The Data From button in the measurement row performs the same function as the Acquisition > Data From menu item; see Input menu.

See Also

Available Properties and Controls

Measurements Dialog