About Downlink Channel Parameters (NB-IoT)
The Downlink Channel Properties dialog contains power boost and channel assignment controls for downlink frame transmission.
Power Boost - Sets the power boost level for each downlink physical channel or signals. NPDSCH power boost is separately controlled under Channel Configuration.
- NRS - Narrowband Reference Signal
- NPSS - Narrowband Primary Synchronization Signal
- NPRS - Narrowband Positioning Reference Signal
- NSSS - Narrowband Secondary Synchronization Signal
- NPDCCH - Narrowband Physical Downlink Control Channel
- NPBCH - Narrowband Broadcast Signal
- CRS - Cell Reference Signal
Subframe Channel Assignments - Assigns a downlink physical channel to each subframe by index (0:19). Some subframes have fixed channel assignments per the NB-IoT standard, as shown in the illustration below. The remaining subframes can be assigned either NPDCCH or NPDSCH.
See Also