Operation Mode (NB-IoT)
selects between modes of operation for the NB-IoT carrier.
- In-Band (same PCI)(downlink): In-band deployment. The NB-IoT carrier shares the same physical Cell ID as the E-UTRA UMTS Terrestrial Radio Access: A W-CDMA standard developed ETSI, ARIB and the TIA. This system uses DSSS and either FDD or TDD depending on its frequency assignment and application. carrier.
- In-Band (different PCI)(downlink): In-band deployment. The NB-IoT carrier has a different physical Cell ID than the E-UTRA carrier.
- In-Band (uplink): In-band deployment.
- Guard Band: Guard-band deployment.
- Standalone: Stand-alone deployment.
Default: Standalone
Choices: In-Band (same PCI)(downlink), In-Band (different PCI)(downlink), In-Band (uplink), Guard Band, Standalone
See Also