RS Tx. Power (Avg) (NB-IoT)
is the average NRS signal power on the reference measurement channel for the data in the Measurement Interval. This data result can be used to calculate RSTP as defined in the standard.
This data result is only applicable to downlink signals.
is calculated by summing the powers of all resource elements occupied by NRS on the reference measurement channel in the and dividing by the total number of resource elements in the .
is expressed in dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer.
See Also