Measurement Interval (NB-IoT)
20 slots, 0 symbol-times
determines how much data is sent to the demodulator and can be specified in slots (SymGroup for NPRACH) plus symbol-times. The beginning of the measurement interval is specified as an offset from the Analysis Start Boundary. The offset is specified by the Measurement Offset parameter. Measurement Interval, Measurement Offset, and Result Length are always specified in slots with the length that matches the detected subcarrier spacing (15 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). Þ 0.5 ms, 3.75 kHz Þ 2 ms).
The Time Offset data result in the Error Summary trace shows the distance from the beginning of the Search Time trace to the beginning of the measurement interval.
See Also