IQ Meas Time (NB-IoT)
shows the same information as IQ Meas when the data is shown in the or trace format. When the data is shown in any other format, time is on the horizontal axis instead of frequency as in .
The information in the IQ Meas topic applies to , with the exception mentioned above.
See Also