About 5G NR/5G-Advanced Modulation Analysis

89601BHNC (89601B-BHN) adds 5G New Radio/5G-Advanced and Pre-5G modulation analysis capability to your 89600 VSA software. With 89601BHNC (89601B-BHN), you can demodulate 5G NR and 5G-Advanced signals that comply with the following 5G NR standards.

* The VSA software doesn't distinguish between the 15.7.0 and 15.8.0 versions because only minor corrections were made between the two versions.

See Also

Setting up a 5G NR/5G-Advanced Measurement

Selecting 5G NR/5G-Advanced Demodulation

5G NR/5G-Advanced Demod Properties Dialog Box

Troubleshooting