Selecting 5G NR/5G-Advanced Demodulation
Configures the 89600 VSA to demodulate 5G NR/5G-Advanced signals (uplink and downlink) that are compliant with the 5G NR/5G-Advanced technical specifications listed in About Option BHN: 5G NR/5G-Advanced Modulation Analysis.
Configure the demodulator
After selecting the 5G NR/5G-Advanced measurement type, the measurement configuration parameters must be configured. Manually configure desired signal to demodulate using the parameters in the Format tab of the 5G NR/5G-Advanced Demod Properties dialog box.
Example recording
The 89600 VSA includes an example 5G NR signal that can be used to help you learn how to use the 5G NR demodulator. The included signal is listed in the Demo and Recorded Signals topic in the Getting Started book.
See Also
Setting up a 5G NR/5G-Advanced Measurement