Extend Frequency Lock Range (5G NR/5G-Advanced)
Default: Disabled (cleared), 90 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second).
Range: 0 - 1MHz (when PRACH Physical Random Access Channel is enabled on one of the carriers, the maximum value is 3 times PRACH Subcarrier Spacing)
When enabled (checked), increases frequency lock range by +- the value specified in the field to the right of this parameter.
For PRACH, the recommended Extend Frequency Lock Range setting is 2-3 times the subcarrier spacing. Too big of a lock range will seriously slow down the demodulation.
Use this parameter only when necessary. Increasing the frequency lock range may cause the measurement to take longer.
See Also