Signal Repetition Pattern (5G NR/5G-Advanced)
provides parameters for signal repetition pattern analysis.
Repetition Pattern - Selects between a 3GPP-compliant (standard) signal repetition pattern and a custom (per-slot) pattern.
Standard - (default) DMRS repeats every 10 ms and CP 1) Contention period, or 2) Cyclic prefix length repeats every 0.5 ms. Use this setting for 3GPP-compliant measurements.
Per Slot - Each time slot, beginning with the value specified in First Slot, is repeated across the full frame (DMRS and CP length repeat each slot).
Default: Standard
Range: Standard, Per Slot
First Slot - Sets the first slot to be used in per-slot signal repetition analysis (Repetition Pattern set to Per Slot).
Default: 0
See Also