SINR Report (5G NR/5G-Advanced)
- When enabled, SINR Signal to (Interference + Noise) ratio data is used to render a 3D representation in the SINR 3D trace. The data disaplyed in SINR 3D trace can be either from internally measured SINR or from a customer provided SINR report (see Load SINR Report).
When Load SINR Report is clicked, this parameter is automatically checked.
Default: Disabled
Choices: Enabled, Disabled
- Click to open a dialog to select and import a SINR report file (*.st9, *.st9And10).
When Load SINR Report is clicked, SINR From Report is automatically checked.
See Also