Rate Match Patterns (5G NR/5G-Advanced)

Rate Match Patterns opens the PUSCH Rate Match Patterns dialog which allows you to configure up to eight rate match patterns for each PUSCH.

Add Rate Match - Adds a rate match pattern.

Remove Rate Match - Removes the selected rate match pattern.

Clear All - Removes all but the original rate match pattern.

Parameters

Rate Match - Selects a rate match pattern for editing. There is a single rate match pattern (0) by default. Use this parameter along with Add Rate Match, Remove Rate Match and Clear All to manage multiple rate match patterns.

Default: 0

Enabled - Enables or disables the selected Rate Match.

ID - Sets a numerical identifier for the selected Rate Match. ID is automatically assigned when a new Rate Match is added as the lowest available ID value in the 0-7 range of possible IDs.

Default: 0

Range: 0 - 7

Level - Selects whether the rate match pattern is defined on the BWP level or the cell level.

Default: BWP Level

Choices: BWP Level, Cell Level

Subcarrier spacing - Sets the subcarrier spacing for this resource pattern. When Level is set to BWP Level, the subcarrier spacing is always set to the SCS of the associated BWP (default = 30 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second).). When Level is set to Cell Level, the subcarrier spacing is selectable as 15kHz, 30kHz or 60kHz (FR1), and 60kHz or 120kHz (FR2).

Default: 30kHz

Range (FR1): 15kHz, 30kHz, 60kHz

Range (FR2): 60kHz, 120kHz

RB Bitmap Index - Defines the RBs to which the rate match is applied. If an RB's index is included in the RB Bitmap Index field, the rate match is applied to that resource block. RBs are entered as an array of resource block indexes.

Example:

RB Bitmap Index = 0, 3, 120:272

Default: 0:272

Symbol Bitmap Span - Selects whether to set the size of the symbol bitmap to span the length of a single slot (14 bits) or two slots (28 bits).

Default: One Slot

Choices: One Slot, Two Slot

Symbol Bitmap - Sets the symbol-level bitmap in time domain. The length of the symbol bitmap is either 14 bits or 28 bits and is determined by Symbol Bitmap Span. A bit set to true indicates a rate match around the corresponding symbol. The symbol bitmap's recurrence is determined by the Periodicity and Periodicity Pattern Bitmap settings.

Default: 00000000000000

Periodicity - Sets the repetition pattern length (in bits) for the Periodicity Pattern Bitmap.

Default: N1

Choices: N1, N2, N4, N5, N8, N10, N20, N40

Periodicity Pattern Bitmap - Sets the recurring repetition pattern as a bitmap with a length specified by the Periodicity setting. For example, when Periodicity is set to N2, the periodicity Pattern Bitmap's length is two bits. Setting the Periodicity Pattern Bitmap to "10" would create a recurring pattern where rate matching occurs based on Symbol Bitmap, followed by a cycle of non-rate matching.

Default: 1

Affected Parts - Determines which parts of the channel are affected by this rate match pattern.

Data – only data parts are affected by this rate match pattern. In this mode, DMRS in the rate-matched PRB/symbol is preserved and used for channel estimation. This choice may be required for correct demodulation and EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. results with some conformance test cases.

Data and Dmrs – (legacy behavior) both data parts and DMRS parts are affected by this rate match pattern. In this mode, the entire PRB (data + DMRS) is excluded from demodulation.

Default: Data

Choices: Data, Data and Dmrs

See Also

PUSCH Panel

Configuration tab

5G NR/5G-Advanced Demod Properties Dialog Box