CC Signal Capture Mode (5G NR/5G-Advanced)
CC Signal Capture Mode selects the method of configuring the hardware acquisition and channel setup.
Manual- When selected, the user manually configures the hardware acquisition and channel setup.
Auto- When selected, the VSA software tries to automatically configure the acquisition and channel setup. The VSA software will set up either a single acquisition or a sequential acquisition. However, Auto mode always prefers to configure single acquisitions when possible.
The Auto mode can be slow to configure depending on the hardware used. For example, an Infiniium scope without DDC will configure more slowly than a UXA signal analyzer.
Sequential- When selected, the VSA software forces a configuration of one acquisition per CC. See the Sequential Input Channel Acquisition Overview topic for more information.
The Sequential mode can be slow to configure depending on the hardware used. For example, an Infiniium scope without DDC will configure more slowly than a UXA signal analyzer.
Default: Auto
Choices: Manual, Auto, Sequential
See Also