Channel Centers... (5G NR/5G-Advanced)
Channel Centers... (Input Channel Configuration dialog) allows you to set the center frequency of each input channels as well as the measurement's span and acquisition count. These are the same settings that are found in other areas of the user interface. They are consolidated and localized within the 5G NR measurement for convenience.
specifies the width of the frequency band to be analyzed in the 5G NR measurement. This is the same setting found in Analysis > Frequency. See Span for more information.
specifies the number of acquisitions in the measurement. This is the same setting found in Acquisition > Channels > Custom. See Acquisition Count for more information.
specifies the center frequency for the selected input channel. This is the same setting found in Analysis > Frequency, but in a tabular form for easy visualization when multiple input channels are used. See Center for more information.
See Also