Chn (5G NR/5G-Advanced)
The Chn columns display the channel mappings for each carrier, as defined by the Channel Indexes parameter. Each column heading also shows the center frequency for the measurement channel.
The carrier's primary measurement channel is indicated in each row to the left of the Chn columns. If multiple measurement channels are mapped to a carrier, the measurement channel with the lowest index is the primary channel.
See Also