Analysis Region (5G NR/5G-Advanced)
The Analysis Region parameter group controls the subframe configuration for the analyzed signal.
sets the measurement's result length (in subframes). Result Length, along with Analysis Start Boundary, determines the amount of data acquired.
Default: 10
sets the subframe + symbol offset, relative to Analysis Start Boundary. Valid selections will depend on the Result Length, and the Synchronization Type.
Default: 0 Subframes, 0 Symbols
sets the subframe + symbol interval, relative to Analysis Start Boundary and Meas Offset. Valid selections will depend on the Result Length, and the Synchronization Type. This measurement assumes the radio frame start corresponds to a subframe offset of zero.
Default: 10 Subframes, 0 Symbols
See Also