Time/Spectrum/CCDF Data Source (5G NR/5G-Advanced)
All
All, Enabled Channel, EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. Included Channels
determines the data source for the CCDF Complementary Cumulative Distribution Function measurement of burst signals, excluding the OFF power. All Time, Spectrum and CCDF traces use same data source as selected by this parameter.
All - The Time/Spectrum/CCDF data source includes all signals within the Meas Interval, including OFF power, are used as the Time/Spectrum/CCDF data source.
Enabled Channels - The Time/Spectrum/CCDF data source includes data within the Meas Interval, detected active based on channel configurations.
EVM Included Channels - The Time/Spectrum/CCDF data source includes all enabled physical channels within the Meas Interval that are selected for EVM calculation in the Results & Filters panel's EVM Include column.
See Also