Channel Power (Active) (5G NR/5G-Advanced)
Menu Path:
is the average power of the ON part of the 5G NR signal and is calculated in the time domain. The Channel Power (Active) metric is especially useful when measuring TDD Time Division Duplex: A duplexing technique dividing a radio channel in time to allow downlink operation during part of the frame period and uplink operation in the remainder of the frame period. signals.
For consistent channel power results across all traces (Summary, Spectrum, Time, etc.), set MeasSetup > ResBW > Window Type to Uniform (Rectangular).
See Also