Summary (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
The table lists the available component carrier summary data for 5G NR modulation analysis.
When more than one carrier is defined in the Aggregation Table, "(CCn)" will appear in the title of this trace, where "n" is the number of the component carrier whose data is displayed in the trace. Select the desired component carrier number using the Configuration > Carriers > Display parameter.
____________
____________
____________
____________
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.
See Also