Freq Err (5G NR/5G-Advanced)
is the average frequency error of the data in the measurement interval, specified as an offset from the current center frequency setting.
See Also
is the average frequency error of the data in the measurement interval, specified as an offset from the current center frequency setting.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |