In-band Emissions Result (5G NR/5G-Advanced)
Menu Path:
shows the PASS/FAIL results of the auto-generated limit test on the In-band Emissions trace.
displays a delta value and location by Slot and RB. For a PASS result, this delta value is the Narrowest Pass Margin. For a FAIL result, this delta value is the Widest Fail Margin.
refers to the average delta from the limit for a PASS result. For a FAIL result, FAIL is also reported in this field.
In-band Emission result data is also shown in the Markers window when a marker is applied to the trace and Limit Test is enabled with Limit Test from Trace is selected.
See Also