OFDM Sym. Tx. Power (5G NR/5G-Advanced)
Menu Path:
(OSTP) is the average symbol transmit power.
For Downlink, the power is the averaged symbol power over symbols on which only PDSCH Physical Downlink Shared Channel and/or PTRS are transmitted.
For Uplink, the power is the averaged symbol power over symbols on which only PUSCH and/or PTRS are transmitted.
If a symbol contains SS/PBCH channel or DMRS channel, it is not included in the OSTP power calculation.
See Also