Spectrum Flatness Result (5G NR/5G-Advanced)
indicates the overall PASS/FAIL result of the Uplink Spectrum Flatness test. The specific failed tests are indicated in the R1 Ripple Failed Slots, R2 Ripple Failed Slots, Max(R1)-Min(R2) Failed Slots and Max(R2)-Min(R1) Failed Slots results. See the EVM Equalizer Spectrum Flatness trace for pass/fail limits and metrics for each slot.
See Also