Symbol Clock Error (5G NR/5G-Advanced)
shows the frequency error between the measured signal's symbol clock and the reference symbol clock in parts-per-million (ppm). The error is calculated by averaging the symbol timing corrections during the measurement interval.
When the signal contains a very small number of RBs, there is not enough data to reliably calculate Symbol Clock Error and '***' is displayed as the Symbol Clock Error value.
See Also