IQ Imbalance Spectrum (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
IQ Imbalance Spectrum shows the IQ Gain Imbalance and IQ Quad Error across the subcarriers before the IQ impairment compensation.
See Also