UE Reported Metrics Summary (5G NR/5G-Advanced)

The UE Reported Metrics Summary trace shows UE User Equipment (e.g. cell phone)-reported measurement metrics such as RSRP, RSRQ, RSSI Received signal strength indication and SINR Signal to (Interference + Noise) ratio. These metrics are used for procedures such as cell selection, cell reselection, power control calculations, mobility procedures and beam management.

UE Reported Metrics Summary is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.

             
CC Channel Name Resource Measured RSRP (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) RSRQ (dB) RSSI (dBm) SINR (dBm)

Name given to each carrier that is mapped in the carrier aggregation table.

Channels include:

 

SSB

CSI channel state information-RSn

Displays the resource elements within the channel that are used in the measurement.

RSRP is the SS or CSI reference signal received power.

Rows without user data are denoted with '***'.

RSRQ is the SS or CSI reference signal received quality.

Rows without user data are denoted with '***'.

RSSI is the SS or CSI received signal strength indicator.

Rows without user data are denoted with '***'.

SINR is the SS or CSI signal-to-noise and interference ratio.

Rows without user data are denoted with '***'.

See Also

Matrix Tables