BRS Survey (Pre-5G)
The BRS Survey trace data presents the relative magnitude and phase of the detected BRS signals affiliated with different antenna ports within a Control subframe.
NOTE: This trace data is available if Detect Antenna Ports is selected for the BRS physical channel in the Control subframe definition, and if the Control subframe is mapped to a subframe contained in the measurement configuration.
See Also