ESA Measurement Setup Parameters

This topic provides measurement and parameter setup information that is unique to ESA spectrum analyzers with 89600 VSA software. This information will help to properly setup the 89600 VSA software and make measurements for the various ESA with 89600 VSA measurement systems.

If the PSA has option 266 (ESA/PSA Series Programming Code Compatibility Suite) make sure the Remote Language for the PSA is set to SCPI. To see if the PSA has option 266, press the following keys on your PSA: System > More > Show System or send the SCPI command SYST:OPT?. To set the Remote Language to SCPI, press the following keys on the PSA: System > Config I/O > Configure Remote Lang > Language and select SCPI or send the SCPI command SYST:LANG SCPI.

Table of Measurement Setup Parameters for the ESA with 89600 VSA

Alignment/Calibration

Overlap

Channels

Preset

Coupling

Range

External Reference Frequency

Recording

Frequency

Setup Save/Recall

Frequency Bands

Span

Frequency Counter

TD-SCDMA Restrictions

Front Panel ESA Control

Trigger Holdoff

Hardware

Triggering`

Custom Channel Configurations Trig Out

Alignment/Calibration: Selecting Calibrate from the 89600 VSA Calibration dialog box (Hardware > Calibration) will initiate a ESA full alignment. The AMPT REF OUT signal must be connected to the INPUT 50 W connector before selecting Calibrate.

The software also monitors the warm-up status on the ESA. Within 30 minutes from the time the ESA is powered on, if the temperature changes by more than 3 degrees from the temperature at the last calibration, the calibration state is set to WARMUP.

Custom Input Channel Configurations: When using the Input Channel Configuration dialog to specify or modify the input channel configuration mapping, only the VSA default set of channel configuration mappings are allowed; "invalid" channel configuration mappings are disallowed and the "OK" button is disabled "greyed out".

Channels: Only a single RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). channel is available.

Coupling: For RF measurements, only AC coupling is available.

Custom Channel Configurations

The Custom Channel Configurations dialog is used to create custom channel mapping configurations, that is, you can reconfigure the hardware input channel to VSA measurement channel connections. When using the Input Channel Configuration dialog to specify or modify the input channel configuration mapping, only the VSA default set of channel configuration mappings are allowed; "invalid" channel configuration mappings are disallowed and the "OK" button is disabled "greyed out".

External Reference Frequency: The external reference frequency can be set up in two different ways with the ESA and 89600 VSA software. The setup depends on the setting specified for Opt Freq Ref (B7E) under Configure.

Frequency: The limits for frequency parameters are determined by the ESA.

Frequency Bands: The frequency bands represent the settable center frequency limits.  A single band is available, where the settable center frequency limits depend on which model ESA used.

E4402B

0 to 3.1 GHz Gigahertz: A frequency measurement which equals one billion hertz.

E4404B

0 to 6.78 GHz

E4405B

0 to 13.3 GHz

E4407B

0 to 27 GHz

The frequency bands in the above table are what the 89600 VSA software enables the center frequency to be set to.  The lower and upper frequencies of these bands fall outside of the specified AC coupled frequency ranges of the ESAs.  The specified AC coupled frequency ranges of the ESAs are:

E4402B

9 kHz kiloHertz: A radio frequency measurement (one kilohertz = one thousand cycles per second). to 3.0 GHz

E4402B with opt UKB

100 kHz to 3.0 GHz

E4404B

100 kHz to 6.7 GHz

E4404B with opt UKB

100 kHz to 6.7 GHz

E4405B

100 kHz to 13.2 GHz

E4405B with opt UKB

100 kHz to 13.2 GHz

E4407B

9 kHz to 26. GHz

E4407B with opt UKB

10 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second. to 26.5 GHz

Frequency Counter: The ESA uses IF subsampling when Alias Protect is set to False. This can result in aliasing effects if the signal is not band limited to the selected span.

Front Panel ESA control: The Disconnect feature can be used to pause the 89600 VSA software and release its control of the ESA. Then the ESA can be used independent from 89600 VSA software. The 89600 VSA software restores the ESA state that was set before disconnected when the measurement is resumed.

Hardware: ESA is listed as a Logical Instrument in the Analyzer Configuration.

See LAN/GPIB Connection Problems for help with potential problems, such as long startup times and/or unexpected behavior.

Overlap: The ESA does not support overlap processing. However, overlap processing is available during recording playback.

Preset: When setup in the 89600 VSA software is preset, these settings are different from those listed under Preset Setup. (Any parameters not listed here are set to the same value as those listed under Preset Setup.)

Parameter

Default Setting

Range

30 dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer

Frequency

 

Bands 

ESA model dependent:

E4402B: 0 to 3.1 GHz

E4404B: 0 to 6.78 GHz

E4405B: 0 to 13.3 GHz

E4407B: 0 to 27 GHz

Center 

1 GHz

Span 

10 MHz

Start 

995 MHz

Stop 

1.005 GHz

Time Data Zoom/Baseband 

Zoom

ResBW

100 kHz

Time

 

Main Time Length 

38.203125 mSec

Max Overlap 

90 %

Gate on/off 

Off

Length 

1.328125 mSec

 

Range: Range is selected by clicking Acquisition > Amplitude in the 89600 VSA. For the RF input, the range limits are - 55 dBm min to +30 dBm max with 1 dB step size. If the ESA internal 20 dB preamp hardware (option 1DS) is detected, the limits are -75 dBm to +30 dBm with 1 dB step size. The VSA then automatically sets the preamp and attenuator for the ESA in order to satisfy the Maximum Mixer Level setting for the selected Full Scale Range.

For center frequencies above 3 GHz, the minimum range is -55 dBm.

Recording: The VSA can record time data from the ESA hardware to your PC's disk drive. The length of time waveform recording is limited to the time waveform length limit of the ESA.

Setup Save/Recall: The ESA state is not saved when an 89600 VSA application is closed. When a setup is recalled into the 89600 VSA, the ESA state is set appropriately based on the recalled VSA setup.

Span: For the RF input, the maximum span is 10 MHz. The minimum span is < 50 kHz if Alias Protect is True and < 50 Hz if AliasProtect is False. Span resolution is independent from ESA and unchanged from 89640 operation.

TD-SCDMA measurements with ESA:

When Alias Protect is set to False, the ESA uses IF subsampling, which can result in aliasing effects if the signal is not band limited to the selected span.

The Demod: Not enough data. (Measurement step 'Demod' encountered this error) Error Message may show if the current hardware setup could not acquire enough time samples to complete the requested Digital Demodulation measurement.

TD-SCDMA measurements with ESA: The 89600 VSA software cannot perform TD-SCDMA demodulation when the ESA is in the alias protected mode (because of ESA memory limitations and demodulation algorithm latency requirements). When the ESA is in the non-alias protected mode, the result length is limited as follows:

In the alias protected mode, it is possible to make one sub-frame measurements either when the hardware is triggered or correctly or when free-run data happens to align correctly. Triggering must be set up to provide about 250 chips of data before the beginning of the sub-frame, depending on the Frequency Span setting.

Trigger holdoff: Trigger holdoff is not supported with the ESA.

Triggering: The following trigger parameters are available:

Style: Free Run, External TTL, IF Mag (Video)

IF Mag (Video) requires newer Option B7E RF Comms Hardware, HW ID 117. To check for this option:

  1. On the ESA, press System, More, Show Hdwr.
  2. Look for an entry of either B7E: Digital Demod RF or B7E: RF Comms Hardware.

Trig Out

Not all ESA models support the 89600 VSA Trig Out feature.

Refer to the Measurements book "Trig Out" topic's Unsupported Hardware table for more information.

See Also

89611 with Keysight ESA option H70

Input Extensions

ESA Setup as ADC

Enhancing Measurement Speed