Enhancing Measurement Speed with ESA
The following actions will increase measurement speed for 89600 software with ESA.
- Set DisplayUpdates to .
- Use a cardinal span when possible.
- Reduce the number of frequency points to the minimum required for the measurement in order to reduce internal vector sizes and the amount of data to be transferred across the interface from the ESA.
- Turn markers off.
- If using averaging, select Fast averaging.
- Set Alias Protect to False to minimize the amount of data to transfer from the ESA at lower spans.
See Also
Product Overview for 89611 with ESA/H70