Angle of Arrival (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis Tab > Angle of Arrival Panel

The Analysis tab's Angle of Arrival panel lets you enable and configure Angle of Arrival analysis. The angle of arrival (AoA) of a signal is the direction from which the signal is received. To perform this measurement, you need at least 2 channels to calculate the angle.

Antenna Orientation Visual -- Click the expand icon on the right side of the panel to show a Closed3D illustration of the current antenna configuration. See the Antenna Orientation description for additional antenna orientation diagrams.

Right-click on the illustration to rotate the 3D visual around the origin.

The Angle of Arrival panel allows you to set the following parameters:

See Also

Pulse Table