Pulse Table

Menu Path: Trace > Data > Result Tables

The Pulse Table is a type of Matrix Table that includes all pulse-specific result metrics, measured over all valid, synchronized, pulse-analysis time samples detected within the time specified by Acquisition Length (sec), up to the number of pulses set with Maximum Pulse Count.

All displayed metrics in the table (except for Pulse index) are measured over the pulse-specific, synchronized, user-specified analysis time samples as determined by the settings in the Thresholds and Analysis Regions on the Regions tab

When averaging is turned on, the reported metrics are averaged.

You can highlight one row, then right-click and select Set Start Pulse to conveniently set the Starting Pulse.

Selecting Pulses to Analyze from the Table

You can set which pulses the measurement analyzes directly from the Pulse Table, rather than entering values in the Selected Pulses parameters on the Time tab. Select one row, or a range of rows, then right-click the selection and choose one of the following commands.

Rows whose pulses fall within the currently analyzed range are shown in bold, so you can see the range at a glance. No rows are shown in bold when the measurement is analyzing all pulses, because every row is included in that case. Rows outside the analyzed range continue to report their measured results.

These commands and the bold row emphasis apply to the Pulse Table, whose rows are the individual detected pulses. They are not available on the Pulse Cumulative Results Table or other statistics tables.

Exporting Pulse Data

You can export pulse data as a pulse table or as a Pulse Descriptor Word (PDW) file in the File > Export menu.

The Export menu is only visible when the Pulse measurement type is selected. Export choices are grayed out until a pulse table is displayed and selected.

Sorting by metric

You can sort the table by any metric by left-clicking the metric name. Click again to toggle between ascending or descending order. Cancel sorting by right-clicking and selecting "Clear Sort".

See Also

About Result Tables

AoA Metrics

Ch-to-Ch Difference Metrics

Deinterleave Metrics

Droop Metrics

Frequency Hopping Metrics

Frequency Metrics

Levels Metrics

Linear FM Metrics

Modulation Decode Metrics

Nonlinear FM Metrics

Overshoot Metrics

Phase Metrics

Pulse Metric

Ripple Metrics

Scoring Metric

Time Metrics

Time Sidelobe/Correlation Metrics

Triangular FM Metrics