Nonlinear FM (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis Tab > Nonlinear FM Panel

The Analysis tab's Nonlinear FM Frequency Modulation panel lets you configure nonlinear FM pulses. Linear FM must be selected as a Pulse Modulation Type because nonlinear and linear FM pulses are both initially detected as linear FM pulses.

The Nonlinear FM panel allows you to set the following parameters:

See Also

Pulse Table