Increase Speed for Exporting Entire Recording (Pulse)

Menu Path: Analysis > Pulse Properties > Advanced

Increase Speed for Exporting Entire Recording check box removes all but trace A and increases acquisition length to reduce the amount of overhead when collecting pulse data from the recording. The original setup will be restored once the PDW export process is complete.

Increase Speed for Exporting Entire Recording only applies when exporting an entire pulse recording using the Export Pulse Descriptor Word File (Entire Recording)... menu selection under File > Export.

See Also

About Export