Extra Acquisition (Pulse)

Menu Path: Analysis > Pulse Properties > Time

Specifies the number of extra acquisition samples reported before the start of the first valid detected pulse result, and after the end of the last valid detected pulse result. This affects how many additional display samples are made available for viewing within the synchronized Amplitude, Phase, and FM Frequency Modulation versus time trace results.

Increasing the number of Extra Acquisition samples may be required to allow automatic time alignment of user Selected Pulses to the 10% to 90% time trace grid graticules when the Include Extra Data Before and After checkbox is enabled.

When Segmented Capture is enabled, the Acquisition Length (s), Extra Acquisition (samples) and Include Extra Data Before and After properties are all grayed-out (unavailable), since you should specify the desired Segmented Capture mode acquisition length using the separate Segment Length (s) and Segment Count properties.