CC Summary (6GR)

The CC Summary trace is a matrix table with one row per mapped-and-enabled carrier in the carrier aggregation configuration — reporting channel power (absolute and relative to the reference carrier), per-carrier EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., time alignment error relative to the reference carrier, center frequency, frequency and clock error, and cell ID.

This is the cross-carrier comparison view, distinct from the single-carrier Summary trace. For a single-carrier configuration the table has one row.

See Also

Summary

Available Trace Data