Summary (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The Summary trace is the headline results table for one component carrier: channel power, EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., frequency and clock error, sync status, and similar carrier-level scalar results, all in one place. This is the trace most users look at first to answer whether the measurement worked and how good the signal is.

The table lists the available component carrier summary data for 6GR modulation analysis. A result that cannot be calculated for the current signal or measurement setup shows '---' instead of a value.

Channel Power

Channel Power (Active)

OSTP

EVM

EVM Pk

Mag Err

Mag Err Pk

Phase Err

Phase Err Pk

Frequency Error

Frequency Error Worst

Symbol Clock Error

IQ Offset

Time Offset

Sync Correlation

Sync Source

Cell ID

____________

Total TB Count

Error TB Count

BLER

Max. Throughput

Measured Throughput

Measured Throughput Pct

The last six results are the transport block decoding results, shown below a divider in the table. They are available only when PDSCH Decode Mode (for a downlink carrier) or PUSCH Decode Mode (for an uplink carrier) is set to something other than Off (No Bits) or Off (Scrambled Bits).

For a cross-carrier comparison view, see the CC Summary trace. For per-physical-channel results, see the Frame Summary trace.

Querying summary table data results programmatically

To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.

See the How To Query Summary Table Data Results topic for more information.

See Also

CC Summary

Frame Summary

Slot Summary

Available Trace Data