OFDM Channel Summary (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace is a matrix table with one row per measurement input channel (unlike Frame Summary, which has one row per physical channel) — reporting channel power, EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., and time, frequency, and clock error per input channel, each relative to whichever channel is configured as the reference channel. It is most useful for multi-channel-input setups; with a single input channel the table has one row.
See Also