Frame Summary (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The Frame Summary trace is a matrix table (sortable, column-selectable, and export-friendly) with one row per detected physical-channel instance in the frame — each row reporting EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., SINR Signal to (Interference + Noise) ratio, power per resource element, modulation format, number of resource blocks, and similar per-channel results. Use it to see results per physical channel rather than one aggregate number.

This trace is not averaged — it reflects the channels detected in a single acquisition each time.

Frame Summary trace

See Also

Slot Summary

Summary

Available Trace Data