Correction (6GR)
The trace is the correction curve used to correct for the frequency response of the input hardware and the input digital filtering. It is applied to the acquired data to compensate for magnitude and phase anomalies in the analyzer's hardware and software signal processing.
For a more detailed description of this trace, see Correction trace data in the Reference.
See Also