OFDM Eq Ch Freq Resp (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The OFDM Eq Ch Freq Resp trace shows the equalizer-estimated channel frequency response for whichever bandwidth part or physical channel currently has the largest resource-block allocation (falling back to the first enabled SS block if none is active).

The result is tunable via the Advanced tab's Equalizer section — for example, Channel Response Computed Per Slot switches between per-slot overlaid results and a single combined result across slots.

OFDM Eq Ch Freq Resp trace

For the per-antenna-path version, see MIMO Eq Ch Freq Resp.

See Also

Equalizer Settings

Available Trace Data