MIMO Eq Ch Freq Resp (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The MIMO Eq Ch Freq Resp trace shows the per-antenna-path channel frequency response for a MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. measurement — one response per path detected as active (a path is considered active when its power is above the reference path power minus the MIMO detection power threshold), each normalized in power and phase to the reference path.

The result is optimized by the same equalizer training settings as the non-MIMO OFDM Eq Ch Freq Resp trace (see the Advanced tab's Equalizer section).

See Also

OFDM Eq Ch Freq Resp

Eq Condition Number

Available Trace Data