OFDM Meas (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The OFDM Meas trace is the measured constellation for the component carrier — the demodulated symbol points as actually received, plotted in the IQ plane. Compare it against the OFDM Ref trace, the ideal reference constellation the measured points are compared to when computing EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format..

OFDM Meas trace

See Also

OFDM Ref

Available Trace Data