OFDM Ref (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace is the ideal reference constellation computed for the component carrier — what the measured symbols (the OFDM Meas trace) are compared against to derive EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format..
See Also