RE Power 3D (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The RE Power 3D trace is a rotatable 3D surface of per-resource-element power across the resource grid (subcarrier × symbol × power). Drag with the mouse to rotate, zoom, and pan; the right-click menu provides auto-scale, preset snap orientations, and an orthographic camera option.

This trace requires a video card and driver that support OpenGL version 2.1 or higher. If it doesn't render correctly, close it or select another trace tab to bring that tab to the foreground instead.

The trace is shown as pane E in the 6GR_FR1_40MHz demo's default layout:

Demo layout including the RE Power 3D trace

See Also

OFDM Err Vect 3D

Available Trace Data