Slot Summary (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace is a matrix table like Frame Summary, but organized by bandwidth part, frame, subframe, and slot rather than one row per channel instance across the whole frame. Each row reports EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., SINR Signal to (Interference + Noise) ratio, power per resource element, power boosting, modulation format, resource-block count, RNTI, and the peak-EVM location (symbol and subcarrier index). Use it to correlate a result back to a specific slot rather than scanning the whole frame.
See Also